This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T774: data rate

Part Number: SN74AVC4T774
Other Parts Discussed in Thread: SN74AXC4T774

Hello,

We are developing an USB 2.0 camera based on the Onsemi AR0144CS image sensor connected to a Cypress FX2 USB controller CY7C68013A. 
Image sensor works at 2.8V and USB controller at 3.3V so we need to use a level shifter to transfer image data from sensor to usb controller.
Onsemi has suggested us using your SN74AVC4T774 level shifter, but cannot guarantee that it will work because they have not tested it.
Can you tell us if this level shifter can work at the maximum image transfer frequency of 75 MHz (from 2.8V to 3.3V)?

Best Regards