This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G32-Q1: Decaps requirement

Part Number: SN74LVC2G32-Q1
Other Parts Discussed in Thread: SN74LVC2G32

I need decaps requirement for Vcc pin for SN74LVC2G32-Q1 OR gate.

  • See section 10 of the SN74LVC2G32 datasheet:

    Power Supply Recommendations

    […]
    Each VCC terminal should have a good bypass capacitor to prevent power disturbance. For devices with a single supply, a 0.1-μF capacitor is recommended. If there are multiple VCC terminals then 0.01-μF or 0.022-μF capacitors are recommended for each power terminal. It is ok to parallel multiple bypass capacitors to reject different frequencies of noise. Multiple bypass capacitors may be paralleled to reject different frequencies of noise. The bypass capacitor should be installed as close to the power terminal as possible for the best results.

    (This paragraph gets copied into all newer datasheets.)