This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Planning to use Level Translator for SPI interface for translation between 1.2V to 1.8V, planning to use TXB0106 device. Few questions with regard to this
1.Is this good to use
2. Are there any better devices which can support till 50Msps speed on SPI l/f
Please suggest
Regards,
Sudarshan
The TXB is an auto-bidirectional translator, which introduces many limitations. For SPI, better use a unidirectional translator like the TXU0304 or SN74AXC4T774.
At these voltages, the TXB and TXU can do up to 20 Mbps (10 MHz); the AXC, more than 80 Mbps (40 MHz).
Hi Clemens,
SN74AXC4T774 looks good for our usage. we will check it. Thanks to your immediate response
Regards,
Sudarshan