Other Parts Discussed in Thread: SN74AUP2G34, SN74AUP1G125
I have a couple of inquiries and questions about the SN74AUP and SN74LVC family of ICs.
I’m trying to drive and quickly toggle or turn on/off an LED with a 24 MHz, 0 – 3.3V ~40% duty cycle signal, at 6-7 mA and 3.3V VCC with the SN74LVC2G34 and SN74AUPG34 drivers.
The LED used: Vishay VSMA1085600, which has a forward voltage of ~2.55V at 10 mA.
Unclear from the datasheet for the drivers, but by interpolating the values provided, VOH minimum should be over 2.55 if VCC is 3.3V and target drive current is 6 mA.
When driving the LED directly with an MCU output, and using a 15 Ohm resistor in series, the current draw is about 6 mA with the required brightness. However, when the MCU output is connected to the SN74LVC2G34 or SN74AUP2G34 input, and the driver output to the LED with the same resistor in series - the current draw not only becomes huge (20 mA and 5 – 10 mA respectively), but the brightness is also low for SN74AUP2G34. Only one input pin is used for now, the other is tied to ground. Not sure what the load capacitance of the LED is. The static current consumption is negligible and the dynamic current consumption for the drivers should be dictated by the below equations. For the SN74LVC2G34 and assuming 30 pF LED load (which may be an over estimation) this should be:
P_T = Cpd*Vcc*fi*N_sw = 15pF*(3.3V)*24MHz 1 = 1.188 mA
P_CL = C_L*fo*Vcc = 30pF*24 MHz*(3.3V) = 2.376 mA
Total = 3.564 mA
For the SN74AUP2G34 this same calculation yields 2.717 mA
Any ideas what could cause the increased current consumption?
Unrelated but according for the datasheet the SN74AUPG106 and SN74AUPG206 the Cpd is 1 pF and 4.3 pF respectively, while for the SN74AUPG107 and SN74AUPG207 it is the other way around, 4.3 pF and 1 pF respectively. Is this correct?
Also the for the SN74AUP1G125 it says on page 5 that the maximum current should be 4 mA, however on page 17 it says that it can drive an LED up to 24 mA at 3.3v. Which one is correct? Does this hold for all AUP family ICs?
Schematics for reference