Other Parts Discussed in Thread: SN74AXC4T774
Hi ,
In my design I using SN74AVC4T774 between MCU to SPI peripherals.
In my design the inputs of the SN74AVC4T774 are placed in Hi-Z when my MCU is in reset.
In the data sheet of the SN74AVC4T774 it is written:
"
Since this device has CMOS inputs, it is very important to not allow them to float. If the inputs are not driven to
either a high VCC state, or a low-GND state, an undesirable larger than expected ICC current may result. Since
the input voltage settlement is governed by many factors (for example, capacitance, board-layout, package
inductance, surrounding conditions, and so forth), ensuring that they these inputs are kept out of erroneous
switching states and tying them to either a high or a low level minimizes the leakage-current
"
I like to know if I need external pull-up or pull-down resistors to the SN74AVC4T774 in my design.
Thanks,
Avi.