This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The cover of the SN74LV1T04-Q1 datasheet says inverter gate.
The inversion sign is missing from the diagram on page 1.
Also see table 7-1 on page 13. In the function table, input H -> output H
It is input L -> output L.
When an actual sample is received and tested, the output signal is output as an inversion of the input.
Isn't the datasheet wrong?
Hi Hyeongseok,
Thanks for bringing to out attention as this would mean that there is an error and I have reached out internally to double confirm and help update accordingly, thanks.
Best Regards,
Michael.