This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T04-Q1: Is the SN74LV1T04-Q1 IC output inverted or non-inverted?

Part Number: SN74LV1T04-Q1


The cover of the SN74LV1T04-Q1 datasheet says inverter gate.
The inversion sign is missing from the diagram on page 1.
Also see table 7-1 on page 13. In the function table, input H -> output H
It is input L -> output L.
When an actual sample is received and tested, the output signal is output as an inversion of the input.
Isn't the datasheet wrong?