This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: Confusion data rate in TXS0102 datasheet

Part Number: TXS0102
Hi,

I am confusing little bit datasheet parameters.

For the timing requirements data rate given in 6.6, the maximum speed is given as 21 Mbps (push-pull) and 2 Mbps (open-drain).
However, in switching characteristics (6.9), the same speeds are given as a minimum with the maximum data rate parameter.




1) How should I interpret this parameter?

2) What is the difference between timing requirement and switching characteristics?
Do the requirements for the timing signal and the switching characteristics describe the features of the level shifter?

Thank you.