This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to use part #TXS0108EQPWRQ1 to shift signals from 3.3v to 5v. I have VCCA connected to 3.3v and VCCB connected to 5v. OE is connected to 3.3v as well to always enable the LS. I am noticing that the b side outputs always have roughly 2.6V on them even when there is no signal going into the corresponding A pin. It only goes to 0 V when the corresponding A pin is grounded. Is this by design? How can I resolve this?
Hi Jacob,
Please see Effects of pullup and pulldown resistors on TXS and TXB devices documenting this behavior similar to what Clemens' has mentioned.
Regards,
Jack