This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS595-Q1: Absolute Maximum Ratings of OE

Part Number: SN74HCS595-Q1
Other Parts Discussed in Thread: SN74LV595A-Q1, SN74AHC595-Q1

Tool/software:

Hello!

What is the rated voltage of the OE pin when VCC is 0V?

Since OE is active low, I plan to pull it up to 5V with 10kΩ outside the IC.

Is it OK if the Absolute Maximum Ratings of IIK is satisfied when VCC is 0V?

     5V / 10kΩ = 0.5mA < 20mA

thank you.