Other Parts Discussed in Thread: SN74LVC1G123
Tool/software:
Hi Team,
I have searched related answers but it seems not accurate enough to solve these questions. Please help with these questions below:
[Q1]The three-temperature accuracy of the tw parameter in SN74LV123A-Q1 is 10%. Has the three-temperature error and accuracy of the Cext capacitor been considered?
[Q2] What factors on the chip side cause such a large tw error of the chip?
[Q3] Under ideal conditions, what is the tw error range of the device under three temperatures (only considering VCC power supply of 5V)?
[Q4] If R=150kΩ, C=30nF, is there any risk in this application condition? (There is no way to make the resistor so large. The capacitor is selected with 2% accuracy of COG, and the maximum capacitance can only be 10nF)
Thanks!