Other Parts Discussed in Thread: TXU0104-Q1, TXB0104
Tool/software:
Hi Expert,
My customer Li-Auto is using this device for level shifting between MCU and SoC in IVI platform. Below is the simplified diagram and schematic:
(BTB is a connector.)

The phenomenon is MCU side cannot pass high-level CS signal to SoC side.
1. Here is the waveform tested when R3 is disconnected. We can see MCU side is driven low after VCCA side is powered up.
bluish-purple line: VREG_MDPX3_1P8
pinkish-purple line: CS signal on R1
blue line: tested on R2

2. If R2 is disconnected, then high-level can be translated to A side.
3. If directly connecting R1 and R2 together, then high-level can be passed to SoC side.
Is this related to MCU driving strength?
And seems that the BTB connector affects translating direction.
Can you help to give some suggestions on this?
Best,
Jiahao