This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUC16245: Fast bus switching or selection in a 1v8 to 3v6 system

Part Number: SN74AUC16245
Other Parts Discussed in Thread: TXV0106, LSF0002, TMUX1574, TS5A23157

Tool/software:

I am designing a new system to validate a new device. My design has 2 interfaces that use i2c and SPI.

I need to be able to drive those interfaces from one of two sources. I would select the source via software.

I would like the SPI interface to run at 50 MHz so I would like the prop time of the device to be as low as possible.

On the i2c side, the prop time can be less since that interface runs at 400 KHz.

I have been looking at the AUC family but that appears only work with 1v8 to 2v7. 

Is there a better solution?

Bill