Part Number: SN74LVC244A
Other Parts Discussed in Thread: SN74LVCH244A, SN74LVC541A
Tool/software:
Hello,
Requesting a response to my query.
Background:
I'm using a SN74LVC244A octal buffer on a daughter board connected to a unidirectional parallel data bus. The buffer's output enable (OE) is asserted when the bus is active and address bits matches. However, the bus signals sometimes go into a tristate state due to multiplexing and buffering on the host board.
My question is: Can I safely leave the inputs to the octal buffer in a tristate/floating state while the IC remains powered but the output enable is deasserted?
Thanks & regards,
Abin
Notes:
1) I'm using a buffer instead of bus switch as the bus signals need to drive multiple ICs.
2) I guess the the below note is for ICs during its operation and not while it is disabled.