This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPLD1201-DGS-EVM: IO9 output H during startup?

Part Number: TPLD1201-DGS-EVM

Tool/software:

Hi,

I think that IO9 output H pulse during startup EVM. Is it true?

Both DFFs has L intial state, so will start L outputs for IO6 and IO7.

But after clicking [CONFIGURE] at the InterConnect Studio, IO6 is H, and IO7 is L, actually.

It seems only DFF0 receive clock pulse from IO9 during startup sequence.