This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
We wanted to investigate the SN74HCS86; we chose the SN74HC86 for comparison.
The results were less than 1mA for all ICs, but the HCS86 had twice the VCC-pin throughput current of the HC86.
Is this a correct representation of the value in the actual device?
The SN74HC86 model is older than PCN#20200629000.1, so I do not expect it to model the typical characteristics of the new die correctly. I'd expect the new HC device to have shoot-through currents similar to that of the HCS. If you want to be sure, you have to actually measure a real device.
I thought the HCS family was superior to other CMOS in shoot-through current performance.
I wanted to corroborate that with this simulation. But the results are the opposite of the promotional phrase on the datasheet.
HCS86 appears to perform worse... The HC86 seems better!