I saw the following parameter in the SN74LV125A datasheet which was not in the SN74AHC125 datasheet. Is the SN74AHC125 capable of the same thing or is only the SN74LV125A capable of having a voltage present on the output when the device is unpowered?
Voltage range applied to any output in the high-impedance or power-off state, Vo (see Note 1)....... -.05V to 7V
Also, are there recommended packages (in terms of availability) for the SN74LV125A and 125AT?