This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A5223 i am using this for switch between 2 power for SD card . but i am facing problem ie... VCC_EX_3v3 is the input and SD_sel is "0" then the output should be NC1 = VCC_EX_3V3 and NO1 = 0 but iam getting NC1= 3.3V and NO1= 2.9V ... i dont