This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm looking for a level translator that can convert an RGMII interface running at 125MHz to/from 1.8 and 2.5V.
One candidate I see is SN74AUC245, do you know if it can be used for RGMII at the above voltages? if not, do you have other recommendations?
Thanks,
The 100MHz comes from "F @ Nom Voltage (Max) (Mhz)" parameter here: www.ti.com/.../description
Hi Jennifer,
320Mbps(Mega bit per second) is mentioned in the datasheet.Is this the data rate per channel of level translator? For example 320Mbps for A1 to B1 pin translation?
Regards,
Bhavya
Hi All,
Please see the new TXV level-shifter family (TXV0106-Q1 / TXV0108-Q1) supporting high-bandwidth timing-margin sensitive interfaces such as RGMII.
For more information, see Enabling high performance interface translation | Video | TI.com, thanks.
Best Regards,
Michael.