Hello,
I would like to clarify some doubts with SN74AVCT4T234
- If VrefA=2.5V and VrefB=1.8V, is it possible to input a signal with 3.3-logic to convert it to a 1.8-logic signal?
- Just to make sure I am not missing anything... to accomplish the conversion, it is only necessary to set the VrefA to the desired output voltage, no pull-up resistors are required, it's ok?
Thank you for your help
Regards