This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About Ron data of SN74CBTLV3257, If you have the following information, please let me know.
・Dispersion data in the process
・Chart of Vcc~Ron
Especially, I want Ron data of Vcc=3V.
①VCC=3V, VI= 0V, II=24mA
②VCC=3V, VI=2.4V, II=15mA
Best regards,
Satoshi
Hi Satoshi, the closest data we have is on the application note http://www.ti.com/lit/szza030, on page 37/38. The data describe the device SN74CBTLV3125 but the performance should be the same as the SN74CBTLV3257 since they are in the same technology family.
-Ryan