This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC04 / About the input voltage range(Absolute).

Other Parts Discussed in Thread: SN74HC04, SN74AHC04

Hi all.

I would like to know the absolute input voltage range of SN74HC04.

If the device isn't powered on (Vcc=0V),
is the device no problem when 5V input voltage is applied to the device?

Best Regards,
Sho Ogane

  • The SN74HC04 has a maximum input voltage of Vcc. If your Vcc = 0 V, the maximum input voltage is also 0 V. Damage can occur if voltages above the maximum are applied.
    If you are looking for a similar part that has over-voltage tolerant inputs, try SN74AHC04.
    Is there a particular application I can help you find a part for?