Hi,
I designed a board with SN74LVC541A as a logic voltage converter for SPI.
In order to get steady idle states, I put pull-down resistors with value of 20K at all the input pins.
After the chip is enabled, I applied a square wave of 500Hz (from a signal generator with 50 Ohm output) at inputs of SN74LVC541A, and measured this input signal with scope, but the input became a flat ground.
Then I removed pull-down resistor, did the same test, now I got a very good square wave output.
Pull-down resistors are forbidden at input for SN74LVC541A?
Thank you,
Shiwei