This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BJT Transistor Selection



Greetings:

I have a simple application that requires a BJT NPN transistor.  Collector-emitter voltage rating 15V or greater is fine.  Collector current 10ma or greater is fine.  VCE (sat) 0.4V or less is fine.

The key parameter needed is that the emitter-base breakdown voltage must be 12V or greater.  I need an SOT23 package.

Please advise.

Carl Reese

214-794-4897 cell;