This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
is there an IC in TI portfolio that I can use to digitially control for switching/multiplexing on / off RS232 signals?
In my search, I wasn't able to find one due to negative voltage level requirements for RS232
I have an application where multiple controller modules are connected serially. Each controller acts as a uart forwarder and thus the system can scale up / down without any problems
I am looking for a fail safe mechanism for the case where a controller module fails to function properly due to a problem (MAX232 chip dead) and kills the communication with the rest of the healthy, functioning modules connected to it.
I thought that I can route a bypass track connected to a switch for the RS232 signals and then in case a problem occurs, the switch can be turned on automatically to bypass the problematic controller module.
thanks a lot
rifo
Hello Shreyas,
Thanks for your reply. I am using a Max232 from TI as the RS232 level converter. Which requirements are needed to find an appropriate IC ? If you can tell me then I can write it.
thanks
rifo
Hello Shreyas,
I have checked the datasheet of Max232R and it says that ttl/cmos voltage levels will be converted to IA/EIA-232-F levels for RS232.
thanks a lot
rifo
Rifo,
Because the most common "CM" failure will be it turned off or unplugged, I suggest using a physical relay. Relay normally closed contacts work even when there is no power.
A DPDT relay can bypass the RS232 through the "CM" and remove the 5k load of the bypassed receiver.
The driver outputs are still connected but won't be a problem unless the driver output is shorted.
Here is a drawing, (ignore pin numbers)