This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ TXS0102 ] Level Translator for MDC and MDIO

Other Parts Discussed in Thread: SN74AVC2T45-Q1, SN74LVC2T45-Q1, TXS0102-Q1, TXS0102, LSF0108

[ TXS0102 ] Level Translator for MDC and MDIO

Hi,

Can you suggest the solution of level translating application for MDIO and MDC signals?

Side-A: 3.3V
Side-B: 2.5V

Since my customer is automotive, so I don't have many options.

SN74AVC2T45-Q1
Automotive Dual-Bit Dual-Supply Bus Transceiver with Config Voltage Translation and 3-State 

SN74LVC2T45-Q1
Automotive Catalog Dual-Bit Dual Supply Transceiver with Configurable Voltage Translation

TXS0102-Q1
Automotive 2-Bit Bidirectional Voltage-Level Translator for Open-Drain and Push-Pull Application

I choose TXS0102, because it seems more like "modern".
Do you have any recommendation and/or comments?


I'm bit concerned that other family such as LSF0108 describe in the datasheet that MDIO and MDC can be supported.
But in the datasheet of TXS0102, there is no descriptions.

Thanks,
Ken

Other reference post

MDIO MDC level translator & buffer [NPI]
e2e.ti.com/.../548148