Hello,
My application calls for a Bi-Directional voltage translator Buffer with the following parameters. On the low voltage side +3.3V the FPGA will drive the line with a 510 Ohm pull-up to 3.3V rail and the output side has a 100 Ohm pull-up to +5V. We are currently using IDT74FCT16245TPAG8 and getting 2V output when the FPGA is driving. I can't check to see what the FPGA sees (on the 3.3V side) when the 5V side is driving. We need at least 2.5V or preferably >=3V on the 5V side when FPGA is driving that line. Do you offer a better solution? I have looked at your FET switches (LSF0108) and they could work for us except the FPGA can't sink more than 12mA.
Appreciate any help you can provide on this.
Thanks,
Mike