This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm using SN74AVC4T774-RGY in a design that can have 0V on Vccb during normal operation. My understanding of the datasheet is that partial power down is supported, and the maximum current consumption in this case should be in tens of microamperes. Unfortunately when I measure it I get much large numbers.
My test setup is: DIR1=DIR3=Vcca, DIR2=DIR4=~OE=GND, A1=A3=B2=B4=GND, 100nF bypass capacitors on Vcca and Vccb. All output pins open. No resistors were used.
In case when Vcca=Vccb=3.3V the current consumption is < 1uA
In partial power down:
Vcca = 3.3V, Vccb = 0V current consumption is 5.4 mA
Vccb = 3.3V, Vcca = 0V current consumption is 4.8 mA
Is such high power consumption expected from this device? And is there any way to improve it?
Regards,
Ievgenii Meshcheriakov
The power consumption is not changing significantly if I change logic levels on A3 and A1 if Vcca=3.3V and Vccb=0V (and B4=B2=0V). There is no current that I can measure flowing in or out of signal pins in this case. Even applying 3.3V to B2 and B4 does not change power consumption and there is no current in or out of those pins too.
Hello Ievgenii,
I tested the setup in the lab, I think I know what is causing your high current consumption. In order to prevent the large current consumption you are getting, all I/O pins must be at GND when either supply is shut off. This is because when either supply is shut off, all I/O pins will be in a high impedance state and can float to unexpected voltage levels. The pins that were initially configured as outputs and did not need to be at GND are no longer configured as outputs when either supply is at GND, so they must be grounded as well.
With all I/O pins at GND, I was seeing .012 uA at VCCA with VCCB at GND and .009 uA at VCCB when VCCA was at GND. With any I/O pins floating, I was seeing several mA of current if either supply was shut off. Try grounding all of your I/O pins and see if this improves your power consumption.