Other Parts Discussed in Thread: SN74LVC1G74, SN74LVC1G04-Q1, SN74LVC2G74-Q1
Hello, TI Team.
Could you please answer the following questions?
1. I'm designing a circuit by applying CD74HCT175.
Please check the attached file.
2. In The Following truth table, Q0 means No change?
SN74LVC1G74 | ||||
INPUT | OUTPUT | |||
/PRE | /CLR | CLK | D | Q |
L | H | X | X | H |
H | L | X | X | L |
L | L | X | X | H* |
H | H | ↑ | H | H |
H | H | ↑ | L | L |
H | H | L | X | Q0 |
3. Please Recommend the Automotive single D Flip Flop with clear and preset and the automotive quad D Flip Flop with reset.
4. SN74LVC1G04-Q1
what is mean the table in p.5 of datasheet?
I apply 3.3V for supply voltage. And Input voltage high level is 3.3V
And then, output voltage high level is 3.3V. is it Right?
Thank you~