This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74GTL2010: Voltage level translation query

Part Number: SN74GTL2010
Other Parts Discussed in Thread: LSF0108, LSF0102

Hi All,

I want to use SN74GTL2010 in my design and my requirements for the voltage translation is as per below:

SREF voltage : 1.8V

DREF and GREF voltage : 2.8V

Number of channel per circuit : 10 bit

Direction sensing : Bidirectional

Sensing type : Auto sensing.

The above parts meets my requirement but according to the datasheet of the part the voltage on the SREF pin should be 1.5V less that the voltage on DREF and GREF pin but in my case i am using 1.8V on SREF and 2.8V on GREF and DREF pin. So can anybody please confirm that will this device will be able to work properly and will be able to translate the signal voltage from 1.8V to 2.8V and viceversa.

Your immediate response will be highly appreciated.