Other Parts Discussed in Thread: SN74HC244, , CD54HC244
Hi,
We are currently using a CD74HC244M96 part (SCHS167E– November 1997 - Revised October 2004) which is required to meet the Human-Body Model test, JEDEC JS-001. I cannot find anything on the datasheet that confirms that this part conforms to this test. However, I have noticed the similar commercial part SN74HC244 (SCLS130E –DECEMBER 1982–REVISED MAY 2016) does conform to this rating at 2kV.
Is it possible to tell me if the CD74HC244 part also conforms to this standard, or what the ESD levels are. Failing this, is there any data avaliable for the protection diodes on the input and output pins to the Vcc and GND rails that are limited to 20mA.
Many Thanks,
Richard
Richard Long
Electronics Engineer – Control Systems
Civil Aerospace
Rolls-Royce
The Derwent Building
5000 Solihull Parkway
Birmingham Business Park
Solihull
B37 7YP