This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVTH245A: Voh MAX

Part Number: SN74LVTH245A

Hi,

SN74LVTH245A

Could you tell me the value of Voh max. (data sheet page4)

I would like to confirm that Voh max does not exceed Vcc.

Best regards

  • Hello,
    The output of the SN74LVTH245A at 0A of current is Vcc.

    That, however, does not preclude the possibility of the output exceeding Vcc. It is very common to see overshoot, often known as 'ringing,' that will exceed Vcc. The amount of overshoot will be linked to the load conditions, and is not a direct result of the output of the SN74LVTH245A.