Other Parts Discussed in Thread: SN74AVC20T245
Hello,
I'm working on a design where I need to interface a 1.8V powered microcontroller to several peripherals (mostly transceivers) that are 3.3V powered.
I have a total of 10 inputs and 10 outputs to shift between the two voltage domains.
When looking at the logic diagram of the SN74AVCH20T245 datasheet, it looks like the device can operate half of its ports independently. Although, since it's not crystal clear, I need a confirmation from you guys.
The way I intent to integrate the device on the design is as follow :
- VCCA = 1.8V, VCCB = 3.3V
- 1DIR = GND, 1OE = GND (in order to have 1Ax/1Bx ports direction set to : B data to A bus)
- 2DIR = 1.8V, 2OE = GND (in order to have 2Ax/2Bx ports direction set to : A data to B bus)
Is this mode of operation correct ?
Thanks in advance for your help !
Stéphane