Hi E2E,
1. The power domain of Pin9~17 is refer to VDDIO(1.7V~3.3V). But the VIH(Max) of these pins is only 1.9V, does it means that these pins only support 1.8V(Class C) input voltage?
If baseband could supply 3V VDDIO(Class B) then it does not make sense that Pin9~17 are limited to 1.9V Max input voltage.
If we need to support 3V(Class B), the VDDIO and Pin9~17 should be supplied in 3V, right?
2.
The System default would start in 1.8V mode, but while the baseband is configuring in 2.95V, there is lack of communication between the baseband and the SIM card, so does the TXS02324 will configure itself to 2.95V automatically or need baseband to control I2C and assert B1=1 in the SIM interface Control Register to finish this voltage transfer?
Does the setting up SIM interface sequence shown as below all depend on Baseband to change register bits to be properly setup?
Thanks!