Part Number: SN74LV07A
I am using LV07 in the switch circuit.
The output pin of LV07 is used in applications where Hi-Z output and Low output are periodically repeated.
However, it may be disturbed by disturbance crosstalk at Hi-Z output.
As an example,
(1) A noise of -800mV (220us) is generated at the output pin.
(2) A noise of -800mV (5us) is generated at the output pin.
It will exceed absolute voltage -0.5V, is there a risk of destruction?
The output pin of LV07 is used in applications where Hi-Z output and Low output are periodically repeated.
However, it may be disturbed by disturbance crosstalk at Hi-Z output.
As an example,
(1) A noise of -800mV (220us) is generated at the output pin.
(2) A noise of -800mV (5us) is generated at the output pin.
It will exceed absolute voltage -0.5V, is there a risk of destruction?