This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVCH20T245: SSO or Crosstalk issues with VFBGA package?

Part Number: SN74AVCH20T245
Other Parts Discussed in Thread: SN74AUCH16244, SN74AUCH244

I am using the SN74AVCH20T245 in the following configuration:

  • Data from B --> A
  • VCCB = 2.5 V, VCCA = 1.8 V
  • 0.1uF, 0402, decoupling cap on each of the 4 power pins, on the backside of the PCB underneath the BGA footprint
  • 16 bits = single data rate data clocked at 156.25 MHz
  • 4 bits =  2 complimentary clock signals at 156.25 MHz

The clocks are always toggling.

In a particular test pattern case, the data bits are static for many clock cycles, then toggle for a few clock cycles.  Think of it like a data packet with a static payload, but a changing header with each packet.

During the static data portion of the packet, the clock signals look normal.  However, when all 16 bits of the data begin to toggle, the P-side clock signals (only, not the N-side) show dramatic amplitude droop for ~3 clock cycles.  So much of a droop that the receiving FPGA (connected to the HA01P/N signals in the above picture) do not register a clock transition.

I have read app note szza029b that describes the simultaneous switched output & crosstalk behavior of the VFBGA package and it looks reasonably good. 

Any tips on where to look for the root cause of this issue?  Thanks!