This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I'm trying to figure out what's the output power of the SN74LS624 VCO.
On the datasheet it's mentioned that V_oh=3.4V typ.
does it mean that if we use it on 50ohm we will get about 14dBm of output power ?
Best regards,
Nir.
This device use standard LS outputs (see page 5 of the datasheet). Input and Output Characteristics of Digital Integrated Circuits at 5-V Supply Voltage (SZZA008) shows typical characteristics:
So a load of 50 Ω would see a high-level voltage of about 1.35 V, which results in about 36 mW, which is indeed about 15 dBm.
Please note that the characteristics are not guaranteed at high-level currents of more than 1.2 mA, and that low and high currents are not symmetrical. For most 50 Ω applications, you would want to add a driver designed for such an impedance.