Other Parts Discussed in Thread: SN74LVC2T45-Q1
Hi Team,
I am using SN74LVC8T245-Q1 8-bit dual supply bus transceiver to interface serial flash (3.3V logic) to controller at 5V supply.
The device SN74LVC8T245-Q1 has direction-control (DIR) input & Output Enable (OE#) input to enable either of the output ports, i.e., A or B.
1. Please elaborate how these pins work/ share application note if available.
2. Is it possible to use few of the A port pins as input & the remaining as output with the same device? same with the port B.
Thanks,
Prachi