This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: Vccb pins 23 & 24: Can pin 23 be left floating?

Part Number: SN74LVC8T245
Other Parts Discussed in Thread: SN74LVCC3245A

I have a customer who would like to replace their SN74LVCC3245A with the SN74LVC8T245 device.

He doesn't want to change the board layout.

Both devices are basically pin-compatible.

However, the current device, SN74LVCC3245A, has Pin-23 as a NC pin.

But the SN74LVC8T245 device has Vccb for Pin-23, AND Pin-24.

Is it possible to leave Pin-23 floating? Or is this necessary to power a different section of internal circuitry, and leaving it floating would cause undesirable effects?