Other Parts Discussed in Thread: SN74AHC245, SN74LVC8T245, SN74LV126A
Hi there-
I'm trying to take a 3.3V microcontroller and communicate with some very old legacy 5V TTL signals. Initially, I was tempted to use the SN74LVCC3245A but I noticed through another forum post that it must have a HI level input voltage minimum of 3.5V.
I was able to find some uni-directional level shifters and/or buffers that are able to act as either a bank of inputs or outputs, but cannot be switched. This application requires re-configuring the part to be bi-directional via the microcontroller (using a direction pin) since there are many different confgurations that the system needs to accommodate.
Given these requirements, would you have a part to suggest or perhaps a tweak to the SN74LVCC3245A circuit that would allow it to accept these TTL signals without being overly complex or expensive?
Thanks!
Dave