Are there any of the 74HC646/647/648/649 logic type that are available in a DIP option? Note the logic family (i.e. 74HC, 74LVC, 74AHC, etc. )doesn't matter for my project and what I am basically looking for is the bidirectional latch or flip flop with tristate outputs available in a DIP format and having at least 8 bits width. If necessary I could make do with the 74HC646 and SMT to DIP adapters but I would much rather simply have a DIP IC.
Thanks for any help.