Part Number: SN74LVC1T45
Other Parts Discussed in Thread: TMUX1511, SN74AHC125, SN74AVC2T245, SN74LVC2T45
Hi,
My project includes a CPLD which is connected to external IOs. Each IO can be set as INPUT or OUTPUT - at 10MHz.
I have to implement a bi-directional level shifting between the two sides. Each of them can be set to a different voltage level: 1.8V/2.5V/3.3V/5V (although the CPLD will be probably set only to 3.3V)
TI's SN74LVC1T45 device is good solution, but because I have to implement a current limit of 10mA to each IO, I need a similar device but with OUTPUT ENABLE.
The DIR (direction) pin is required. I can't use the auto-direction sensing devices.
Is there any good candidate device for this design?
Thanks,
Yaron.