Part Number: LSF0204D
Other Parts Discussed in Thread: SN74AVC4T774
Hi Team,
My customer is searching for the SPI level shifter solution as require below
1. voltage level : 1.8V to 3.3V
2. SPI speed: 50MHz
3. Low propagation : target 3ns max.
I had survey our solution with above require , seems only LSF0204D fit , however , the propagation delay max is higher than customer spec, so do we have any other solution which can fit above requirement?