This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer is searching for the SPI level shifter solution as require below
1. voltage level : 1.8V to 3.3V
2. SPI speed: 50MHz
3. Low propagation : target 3ns max.
I had survey our solution with above require , seems only LSF0204D fit , however , the propagation delay max is higher than customer spec, so do we have any other solution which can fit above requirement?
Hi Clements,
thanks for feedback, I'm not quire understand what different between propagation delay and propagation delay skew,
could you kindly explain ?
Andy
noted , in this case, customer is referring to propagation delay not propagation delay skew.