Other Parts Discussed in Thread: SN74LVC1G29
Hello,
I need to use a fast decoder to be used in conjunction with an SRAM memory. As times are extremely critical, I looked for a decoder that was as fast as possible and also powered by 5V. The model I found was the SN74LVC1G139D, in the datasheet I observed the following information:
In section 6.6 (Switching Characteristics) it says that for a supply voltage of 5V, recommended operating free-air temperature, and CL = 15pF we have:
0.8 ns <= Tpd <= 3.6ns
Figure 1 of section 7 (Typical Characteristics) shows a graph, Propagation Delay x VCC, which shows Tplh and Tphl for the different paths within the decoder. According to the graph, for VCC = 5V the typical time would be close to 2 ns
The following questions arose that I would like to clarify:
- Using 5V supply, what would be the typical time propagation delay ?
- Within the minimum and maximum Tpd range, how Tpd behaves and what influences it? Is it random?
- What to do for Tpd to be closer to 0.8ns?
Another important question:
Is there a version or a similar decoder that have a Enable Low pin on it ?
Wit my best regards,
Daniel.