Other Parts Discussed in Thread: TXB0302
Hi
I wish to use LSF0101 as Level Translator for Platform Environmental Control Interface (PECI).
Its a single wire, bidirection interface operating up to 1MHz speed.
Level translation required is from 1.05V (PECI HOST) to 1.8V (PECI Client).
Please note that the interface will always have a week pull down on the bus.
Host and device communicate by Pulling up the line. The logic bits are decided based on how long the lines are pulled up.
Please share your comments on this application scenario for LSF0101.
Thanks
Sanjeev G