Part Number: CD4047B
Hi team,
Could you provide the power solution and ref design for the specs below, thanks!
1. Input voltage: DC 3.3V to 12V
2. Output voltage: AC +-48V with 50 Hz
3. Max output power: 3W
Best regards,
Sam Ting
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Sam,
These are digital logic devices, i think you are looking for an op amp.