Other Parts Discussed in Thread: SN74LVC1G125
Hi team,
I have some questions about SN74LVC1G125-Q1.
As below image.
My question is
1. Why do we have two Vcc condition. I mean when condition1 Vcc = 1.65V to 5.5V and the IOH = -100uA but there is also a condition2 Vcc = 1.65V and the IOH = -4mA. Does it mean we could modify the IOH and IOL?
2.What is the relationship between IOH and VOH(min)
3. If my customer need SN74LVC1G125 output fullfill VOH>3V and VOL<0.3V, how could I achieve it? (Vcc = 3.3V)
Regards,
Roy