This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC02A: Temperature clarification of SN74LVC02ARGYR

Part Number: SN74LVC02A

Hi team,

1. What is the recommended Ta,max of SN74LVC02ARGYR? 

2. What is the recommended Tj,max of SN74LVC02ARGYR? 

3. What is the absolute Tj,max of SN74LVC02ARGYR? 

4. Please find below two max temperatures - which one is correct? both are referring to Ta? 

Datasheet page 1: Ta up to 85C

Datasheet page 7: Op Temp up to 125C