This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC4020: Unused Outputs

Part Number: SN74HC4020

If some of the outputs of the device are not needed, what kind of termination can be used?

It looks like this device uses LSTTL logic...and the DS mentions literature SCBA004, and that states unused inputs should be tied to VCC/GND via 1~10kΩ resistor.

But what about the unused outputs?

Regards,

Darren